FB#.STOREMULTITURN.ENABLE
Description
This keyword enables or disables the store multiturn feature.
To prevent rollovers, set FB#.STOREMULTITURN.ENABLE = 1. Whenever the drive is power cycled after passing multiturn rollovers, the drive will keep track of the rollovers and retain the correct position.
Enabled | |
---|---|
0 (default) | Disabled |
1 | Enabled |
Context
See Store Multiturn
Versions
Action |
Version |
Notes |
---|---|---|
Implemented |
02-08-03-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
0, 1 |
Default Value |
0 |
Data Type |
Integer |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
|
---|---|---|---|---|---|---|---|
FB1.STOREMULTITURN.ENABLE |
3500h |
0fh |
Unsigned8 |
- |
- |
Read/Write |
No |
FB2.STOREMULTITURN.ENABLE |
3501h |
0fh |
Unsigned8 |
- |
- |
Read/Write |
No |
FB3.STOREMULTITURN.ENABLE |
3502h |
0fh |
Unsigned8 |
- |
- |
Read/Write |
No |
FB4.STOREMULTITURN.ENABLE |
3503h |
0fh |
Unsigned8 |
- |
- |
Read/Write |
No |
FB5.STOREMULTITURN.ENABLE |
3504h |
0fh |
Unsigned8 |
- |
- |
Read/Write |
No |
Name |
ID |
Hex |
Data Type |
Access |
Units |
---|---|---|---|---|---|
FB1.STOREMULTITURN.ENABLE |
30460 |
76FC |
Unsigned8 |
Read/Write |
- |
FB2.STOREMULTITURN.ENABLE |
30461 |
76FD |
Unsigned8 |
Read/Write |
- |
FB3.STOREMULTITURN.ENABLE |
30462 |
76FE |
Unsigned8 |
Read/Write |
- |
FB4.STOREMULTITURN.ENABLE |
30463 |
76FF |
Unsigned8 |
Read/Write |
- |
FB5.STOREMULTITURN.ENABLE |
30464 |
7700 |
Unsigned8 |
Read/Write |
- |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
FB1.STOREMULTITURN.ENABLE |
30460 |
Unsigned8 |
Read/Write |
- |
FB2.STOREMULTITURN.ENABLE |
30461 |
Unsigned8 |
Read/Write |
- |
FB3.STOREMULTITURN.ENABLE |
30462 |
Unsigned8 |
Read/Write |
- |
FB4.STOREMULTITURN.ENABLE |
30463 |
Unsigned8 |
Read/Write |
- |
FB5.STOREMULTITURN.ENABLE |
30464 |
Unsigned8 |
Read/Write |
- |